TMT84

The Profile 3.01 GSD file "EH3x1551.GSD" is fully compatible to the Profile 3.02 device (Firm-/Softwareversion 1.01.zz)!

Using only the new Profile 3.02 GSD "EH021551.GSD" in mixed systems (TMT84 devices with Profile 3.01 and Profile 3.02 ) a modification of the GSD is required.
Refer to the manual, chapter "5.3.3 - Current device description files". 


TMT162

The Profile 3.01 GSD file "EH3x1549.GSD" is fully compatible to the Profile 3.02 device (Firm-/Softwareversion 1.01.zz)!

Using only the new Profile 3.02 GSD "EH021549.GSD" in mixed systems (TMT162 devices with Profile 3.01 and Profile 3.02) a modification of the GSD is required.
Refer to the manual, chapter "5.3.3 - Current device description files".