******************
IMPORTANT:
The CML18_Readout_Tool.exe can be started and run without admin rights.
The tool is self-explaining and shows upon startup brief instructions.
It also includes a little help menu explaining all further steps for downloading a log file.

Please make sure that the following requirements are met for downloading log values:
- Connect the "M12-USB Data and charging cable" to CML18 and to a free USB port of your Windows PC
- No sensor is connected to CML18
- CML18 is turned on
- Data logger at CML18 is stopped (Menu -> "Application" -> "Data logger" -> "Data logger")
- "M12 CSV" is OFF (Menu -> "System/Language" -> "M12 CSV")

After starting the CML18_Readout_Tool:
1. Select the corresponding COM-Port the data cable is connected to
2. Select the file location where the log file shall be saved
3. Click on the appropriate button to download the Grab sample log or Continous logs

Supported operating systems:
- Windows 7 or later
******************

V01.00.00
Initial release.